AXIS#.PL.FILTER.FREQ

Description

AXIS#.PL.FILTER.FREQ sets the frequency of a moving average filter on the trajectory position command. When AXIS#.PL.FILTER.FREQ is greater than zero, the filter is active. The filter is applied to all Command Source types, but only active when the drive is in Position Mode.

The filter can only be set to multiples of 4kHz, if a frequency is entered in between multiples of 4kHz the nearest frequency will be used.

Usable frequency settings are: 2000 Hz, 1000 Hz, 500 Hz, 250 Hz, 125 Hz, 62.5 Hz, 31.25 Hz, 15.62 Hz, 7.81 Hz, 3.90 Hz, 1.95 Hz


  • This replaces AXIS#.PL.FILTERTIME.

Versions

Action Version Notes
Implemented 02-05-02-000
Reworked 02-11-03-000 Filter topology changed from 2nd order lowpass to moving average filter, AXIS#.PL.FILTER.Q deprecated as part of this rework

General Information

Type

Read/Write

Description

Sets the position command filter frequency.

Units

Hz

Range

0 - 2000

Default Value

0

Data Type

Float
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
AXIS1.PL.FILTER.FREQ

500ch

0fh

Unsigned32

-

1000:1

Read/Write

No

AXIS2.PL.FILTER.FREQ

510ch

0fh

Unsigned32

-

1000:1

Read/Write

No

Related Topics

Motion Smoothing

Electronic Gearing